CAP#.COUNT

Description

The number of capture events that have happened since the drive powered up. If capture is configured to auto-rearm, CAP#.REARM is 1, then this counter allows you to detect if a capture event has happened.

Examples

Code

-->CAP1.COUNT
0
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Units N/A
Range

N/A

Default Value 0
Data Type Integer
See Also CAP#.REARM, CAP#.STATE
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

CAP1.COUNT

31010

7922

Unsigned16

Read Only

-

CAP2.COUNT

31011

7923

Unsigned16

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.COUNT

31010

Unsigned16

Read Only

-

CAP2.COUNT

31011

Unsigned16

Read Only

-